TCPIP_UDP_BcastIPV4AddressSet Function
C
bool TCPIP_UDP_BcastIPV4AddressSet(UDP_SOCKET hUDP, UDP_SOCKET_BCAST_TYPE bcastType, TCPIP_NET_HANDLE hNet); Returns
true - Indicates success
false - Indicates failure:
invalid socket
invalid socket address type
a broadcast for the specified interface could not be obtained
invalid broadcast type specified
Description
It sets the broadcast address for the socket
Remarks
This function allows changing of the destination IPv4 address dynamically. However, the call will fail if the socket was previously set to broadcast using the TCPIP_UDP_OptionsSet call. TCPIP_UDP_OptionsSet takes precedence.
Preconditions
UDP initialized UDP socket should have been opened with TCPIP_UDP_ServerOpen()/TCPIP_UDP_ClientOpen()(). hUDP - valid socket
Parameters
| Parameters | Description |
|---|---|
| hUDP | the UDP socket |
| bcastType | Type of broadcast |
| hNet | handle of an interface to use for the network directed broadcast Not used for network limited broadcast |