TCPIP_UDP_PacketHandlerDeregister Function
C
C
bool TCPIP_UDP_PacketHandlerDeregister(TCPIP_UDP_PROCESS_HANDLE pktHandle); Returns
true - if the operation succeeded
false - if the operation failed
Description
This function removes a packet processing handler.
Remarks
Exists only if TCPIP_UDP_EXTERN_PACKET_PROCESS is true
Preconditions
UDP properly initialized
Example
TCPIP_UDP_PROCESS_HANDLE myHandle = TCPIP_UDP_PacketHandlerRegister(myPacketHandler, myParam ); // process incoming packets // now we're done with it TCPIP_UDP_PacketHandlerDeregister(myHandle);
Parameters
| Parameters | Description |
|---|---|
| pktHandle | TCPIP packet handle obtained by a call to TCPIP_UDP_PacketHandlerRegister |