TCPIP_UDP_DestinationIPAddressSet Function
C
bool TCPIP_UDP_DestinationIPAddressSet(UDP_SOCKET hUDP, IP_ADDRESS_TYPE addType, IP_MULTI_ADDRESS* remoteAddress); Returns
true - Indicates success
false - Indicates failure:
invalid socket
invalid socket address type
socket is of broadcast type
Description
It sets the IP destination address This allows changing the IP destination address dynamically.
Remarks
The call will fail if the socket was previously set to broadcast using the TCPIP_UDP_OptionsSet call. TCPIP_UDP_OptionsSet takes precedence. The call will fail if remoteAddress is 0. The destination IP address will not be changed.
Preconditions
UDP initialized UDP socket should have been opened with TCPIP_UDP_ServerOpen()/TCPIP_UDP_ClientOpen()(). hUDP - valid socket remoteAddress - valid address pointer
Parameters
| Parameters | Description |
|---|---|
| hUDP | the UDP socket |
| addType | Type of address: IPv4/IPv6 |
| remoteAddress | pointer to an address to use |