TCPIP_SNTP_ConnectionInitiate Function
C
TCPIP_SNTP_RESULT TCPIP_SNTP_ConnectionInitiate();
Description
This function will start a connection to the NTP server.
Preconditions
The TCP/IP Stack should have been inititialized.
Returns
SNTP_RES_OK - If the call succeeded.
SNTP_RES_PROGRESS - If a connection already in progress then another one could not be started.
Remarks
None.