TCPIP_SNTP_TimeGet Function
C
TCPIP_SNTP_RESULT TCPIP_SNTP_TimeGet(
uint32_t* pUTCSeconds,
uint32_t* pMs
);
Description
This function obtains the current time as reported by the SNTP module. Use this value for absolute time stamping. The value returned is (by default) in UTC format: the number of seconds since 01-Jan-1970 00:00:00. This function also returns the current millisecond obtained from a NTP server.
Preconditions
The TCP/IP Stack should have been initialized.
Parameters
| Parameters | Description |
|---|---|
| pUTCSeconds | Pointer to store the current UTC seconds. Could be NULL if the UTC time is not needed. |
| pMs | Pointer to store the current millisecond. |
Returns
SNTP_RES_OK - If the call succeeded and the values are accurate.
SNTP_RES_TSTAMP_STALE error code - If there is no recent timestamp.
SNTP_RES_TSTAMP_ERROR error code - If there is no available timestamp.
Remarks
When SNTP_RES_TSTAMP_ERROR is returned, the time values are meaningless and should not be used.