TCPIP_SNTP_HandlerRegister Function
C
TCPIP_SNTP_HANDLE TCPIP_SNTP_HandlerRegister(
TCPIP_SNTP_EVENT_HANDLER handler
);
Description
This function registers a SNTP event handler. The SNTP module will call the registered handler when a SNTP event (TCPIP_SNTP_EVENT) ovvurs.
Preconditions
The SNTP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| handler | Handler to be called when a SNTP event occurs. |
Returns
Returns a valid handle if the call succeeds.
Returns a null handle if the call failed (an event handler already registered, for example).
Remarks
The handler has to short and fast. It is meant for setting an event flag, not for lengthy processing.
Currently only one event handler is supported. To register a new one, use TCPIP_SNTP_HandlerDeRegister first.