DRV_ENCX24J600_PacketTx Function
C
TCPIP_MAC_RES DRV_ENCX24J600_PacketTx(DRV_HANDLE hMac, TCPIP_MAC_PACKET * ptrPacket); Returns
TCPIP_MAC_RES_OP_ERR - if the client handle is invalid
TCPIP_MAC_RES_IS_BUSY - if the driver is not in the run state
TCPIP_MAC_RES_QUEUE_TX_FULL - if there are no free descriptors
TCPIP_MAC_RES_OK - on successful queuing of the packet
Description
ENCX24J600 Packet Transmit This function will take a packet and add it to the queue for transmission. When the packet has finished transmitting the driver will call the packets acknowledge function. When that acknowledge function is complete the driver will forget about the packet.
Preconditions
The client had to be successfully opened with DRV_ENCX24J600_Open.
Parameters
| Parameters | Description |
|---|---|
| hMac | the successfully opened handle |
| ptrPacket | pointer to the packet |