DRV_ENCX24J600_StatisticsGet Function
C
TCPIP_MAC_RES DRV_ENCX24J600_StatisticsGet(DRV_HANDLE hMac, TCPIP_MAC_RX_STATISTICS* pRxStatistics, TCPIP_MAC_TX_STATISTICS* pTxStatistics); Returns
TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid
TCPIP_MAC_RES_OP_ERR - if the hMac is valid
Description
ENCX24J600 Get Statistics Get the current statistics stored in the driver.
Remarks
Statistics are not planned for the first release.
Preconditions
The client had to be successfully opened with DRV_ENCX24J600_Open.
Parameters
| Parameters | Description |
|---|---|
| hMac | the successfully opened handle |