DRV_ENCX24J600_SetMacCtrlInfo Function
C
void DRV_ENCX24J600_SetMacCtrlInfo(SYS_MODULE_OBJ object, TCPIP_MAC_MODULE_CTRL * init); Returns
None.
Description
ENCX24J600 Set MAC Control Information This function is used to pass in the TCPIP_MAC_CONTROL_INIT information that is used for allocation and deallocation of memory, event signaling, etc. This function is needed to be called so that the driver can enter initialization state when the tasks function is called.
Preconditions
The driver had to be successfully initialized with DRV_ENCX24J600_Initialize.