DRV_ETHMAC_PIC32MACDeinitialize Function
C
void DRV_ETHMAC_PIC32MACDeinitialize(SYS_MODULE_OBJ object);
Returns
None.
Description
This function supports teardown of the PIC32 Ethernet MAC (opposite of set up). Used by tcpip_module_manager.
Remarks
This function deinitializes the Ethernet controller, the MAC and the associated PHY. It should be called to be release any resources allocated by the initialization and return the MAC and the PHY to the idle/power down state.
Preconditions
DRV_ETHMAC_PIC32MACInitialize must have been called to set up the driver.
Example Function
void DRV_ETHMAC_PIC32MACDeinitialize(SYS_MODULE_OBJ object);