DRV_ETHMAC_PIC32MACReinitialize Function

C

void DRV_ETHMAC_PIC32MACReinitialize(SYS_MODULE_OBJ object, const SYS_MODULE_INIT * const init); 

Returns

None.

Description

This function supports re-initialization of the PIC32 Ethernet MAC (opposite of set up).

Remarks

This function is not supported yet.

Preconditions

DRV_ETHMAC_PIC32MACInitialize must have been called to set up the driver.

Example Function

void DRV_ETHMAC_PIC32MACReinitialize(SYS_MODULE_OBJ object, const SYS_MODULE_INIT * const init);