DRV_ETHMAC_PIC32MACStatus Function

C

SYS_STATUS DRV_ETHMAC_PIC32MACStatus(SYS_MODULE_OBJ object); 

Returns

  • SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed

  • SYS_STATUS_BUSY - Indicates that a previous module operation for the specified module has not yet completed

  • SYS_STATUS_ERROR - Indicates that the specified module is in an error state

Description

This function provides the current status of the MAC driver module.

Remarks

None.

Preconditions

The DRV_ETHMAC_PIC32MACInitialize function must have been called before calling this function.

Parameters

ParametersDescription
objectDriver object handle, returned from DRV_ETHMAC_PIC32MACInitialize