DRV_ETHMAC_PIC32MACParametersGet Function
C
TCPIP_MAC_RES DRV_ETHMAC_PIC32MACParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams);
Returns
TCPIP_MAC_RES_OK if pMacParams updated properly
a TCPIP_MAC_RES error code if processing failed for some reason
Description
MAC Parameter Get function TCPIP_MAC_RES DRV_ETHMAC_PIC32MACParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams); This is a function that returns the run time parameters of the MAC driver.
Remarks
None.
Preconditions
DRV_ETHMAC_PIC32MACInitialize() should have been called. DRV_ETHMAC_PIC32MACOpen() should have been called to obtain a valid handle.