DRV_ENCX24J600_PowerMode Function

C

bool DRV_ENCX24J600_PowerMode(DRV_HANDLE hMac, TCPIP_MAC_POWER_MODE pwrMode);

Returns

  • false - This functionality is not supported in this version of the driver

Description

ENCX24J600 Power Mode This function sets the power mode of the ENCX24J600.

Remarks

This functionality is not implemented in the first release.

Preconditions

The client had to be successfully opened with DRV_ENCX24J600_Open.

Parameters

ParametersDescription
hMacthe successfully opened handle
pwrModethe power mode to set