DRV_ENCX24J600_ParametersGet Function

C

TCPIP_MAC_RES DRV_ENCX24J600_ParametersGet(DRV_HANDLE hMac, TCPIP_MAC_PARAMETERS* pMacParams); 

Returns

  • TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid

  • TCPIP_MAC_RES_OK - if the hMac is valid

Description

ENCX24J600 Get Parameters Get the parameters of the device, which includes that it is an Ethernet device and what it's MAC address is.

Preconditions

The client had to be successfully opened with DRV_ENCX24J600_Open.

Parameters

ParametersDescription
hMacthe successfully opened handle
pMacParamspointer to put the parameters