DRV_ENCX24J600_StatisticsGet Function

C

TCPIP_MAC_RES DRV_ENCX24J600_StatisticsGet(DRV_HANDLE hMac, TCPIP_MAC_RX_STATISTICS* pRxStatistics, TCPIP_MAC_TX_STATISTICS* pTxStatistics); 

Returns

  • TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid

  • TCPIP_MAC_RES_OP_ERR - if the hMac is valid

Description

ENCX24J600 Get Statistics Get the current statistics stored in the driver.

Remarks

Statistics are not planned for the first release.

Preconditions

The client had to be successfully opened with DRV_ENCX24J600_Open.

Parameters

ParametersDescription
hMacthe successfully opened handle