10.6.7.6 DEFINED(symbol)
symbol) Return 1 if symbol is in the linker global symbol table and is defined; otherwise return 0. You can use this function to provide default values for symbols. For example, the following script fragment shows how to set a global symbol begin to the first location in the .text section, but if a symbol called begin already existed, its value is preserved:
SECTIONS { ...
.text : {
begin = DEFINED(begin) ? begin : . ;
...
}
...
}