10.6.7.2 ADDR(section)
section)Return the absolute address (the VMA) of the named section. Your script must previously have defined the location of that section. In the following example, symbol_1 and symbol_2 are assigned identical values:
SECTIONS { ...
.output1 :
{
start_of_output_1 = ABSOLUTE(.);
...
}
.output :
{
symbol_1 = ADDR(.output1);
symbol_2 = start_of_output_1;
}
...
}