7.1.30 Fixupoverflow Linker Option
The --fixupoverflow=action option
specifies how the linker will respond should it encounter an overflow when fixing up a
symbol.
Fixup is the process of replacing symbolic references in code with an actual value once
psects have been located in memory and the address or value of symbols have been
resolved. If the linker determines that the value of a symbol is too large to fit into
the space reserved for it in the program image, then this is known as a fixup
overflow. The default action of the linker when
encountering a fixup overflow in C programs built with the xc8-cc
driver is to trigger an error.
--fixupoverflow option customizes the action taken by the linker
when a fixup overflow situation is encountered, as described by the
action arguments in the following table.| Action | Response |
|---|---|
error | Trigger an error message (the
default response when used with
xc8-cc). |
warn | Truncate the value to fit and trigger a warning message. |
lstwarn | Truncate the value to fit and insert a warning marker into the assembly list file where the overflow occurred. |
ignore | Truncate the value to fit and continue with no notification of the fact. |
The warn and lstwarn actions can both be selected with
this option, in which case they must be separated by a colon (:), for
example --fixupoverflow=warn:lstwarn.
-Wa,-a
compiler option and the lstwarn action has
been requested, a warning message will be inserted into the list file before the
instruction or directive that contains the symbol being fixed up. The message will
appear similar
to:13 003FF4 6F14 movwf _bar,b
14 003FF6
warning: (2090) fixup overflow storing 0x202 in 1 byte
5102 movf _foo,w,bwhich shows an
overflow associated with the symbol _foo. In this instance, the symbol
has been resolved to the value 0x202, but there are only 7 bits in the
movf instruction to hold the address offset of the file register
being accessed. The linker has truncated the value 0x202 to a 7-bit quantity (0x02) and
inserted this into the program image forming the opcode 0x5102.If warning messages are inserted into a list file, a single advisory message will be
issued by the compiler for each affected list file to alert
you to this action. If the lstwarn action was specified, but an
assembly list file was not actually requested, then an alternate warning message will be
issued by the compiler.
Fixup overflows in C programs will almost certainly indicate
some sort of error in how the code was written or linked. It is recommended that the
(default) action of error is not change and that any fixup error is
resolved. Selecting an action of ignore, warn, or
lstwarn will allow the program to build, but these actions in no
way address the underlying issue.