7.1.18 P: Position Psect
-Pspec options. The
argument to the -P option consists of comma-separated sequences in the
form:-Ppsect=linkaddr+min/loadaddr+min,psect=linkaddr/loadaddr,...All values can be omitted, in which case defaults will apply, depending on previous values. The link address of a psect is the address at which it can be accessed during runtime. The load address is the address at which the psect starts within the output file (HEX or binary file, etc.), but it is rarely used by 8-bit PIC devices. The addresses specified can be numerical addresses, the names of other psects, classes, or special tokens.
Should the argument to this option contain a comma, you must pass this option to the
linker from either the MPLAB XC8 C compiler (xc8-cc) or the MPLAB
XC8 PIC Assembler (pic-as) drivers using the
-Xlinker driver option (see Xlinker Option) rather than the
-Wl option to avoid the comma being misinterpreted.
-Ptext10=02000hwhich places (links) the
starting address of psect text10 at address
0x2000;-PmyData=AUXRAMwhich places the psect
myData anywhere in the range of addresses specified by the linker
class AUXRAM (which would need to be defined using the
-A option, see A: Define Linker Class Option);
and-PstartCode=0200h,middleCode,endCodewhich
places endCode immediately after the end of
middleCode, which in turn is placed immediately after the end of
startCode, which will start at address 0x200. Note that if you were
to specify a linker class instead of an absolute address in the above example, the
psects listed after the class will also be placed anywhere in the address range
specified by that class. If the link order of the psects is important but the link
address is flexible, use two options. For example, the
options-PstartCode=SEQCODE -PmiddleCode=startCode,endCodewill
place startCode anywhere in the range of addresses specified by the
linker class SEQCODE (which would need to be defined using the
-A option), and the endCode psect will be placed
immediately after the end of middleCode, which in turn will be placed
immediately after the end of startCode.The additional variants of this option are rarely needed but are described below.
If a link or load address cannot be allowed to fall below a minimum
value, the +min, suffix indicates the minimum
address.
If the link address is a negative number, the psect is linked in reverse order with the top of the psect appearing at the specified address minus one. Psects following a negative address will be placed before the first psect in memory.
/ character is supplied with no address
following, the load address will concatenate with the load address of the previous
psect. For example, after processing the
option:-Ptext=0,data=0/,bssthe
text psect will have a link and load address of 0; data will have a
link address of 0 and a load address following that of text. The bss
psect will concatenate with data in terms of both link and load addresses.A load address specified as a dot character, “.” tells
the linker to set the load address to be the same as the link address.
The final link and load address of psects are shown in the map file (see Psect Information Listed By Module).