23.6.2.1 Initialization
The EIC must be initialized in the following order:
- If required, configure the NMI by writing the Non-Maskable Interrupt Control register (NMICTRL).
- Enable GCLK_EIC or CLK_ULP32K when one of the following
configurations is selected:
- The NMI uses edge detection or filtering
- One EXTINT uses filtering
- One EXTINT uses synchronous edge detection
- One EXTINT uses debouncing
GCLK_EIC is used when a frequency higher than 32 KHz is required for filtering.
CLK_ULP32K is recommended when power consumption is the priority. For CLK_ULP32K, write a ‘
1’ to the Clock Selection bit in the Control A register (CTRLA.CKSEL). - Configure the EIC input sense and filtering by writing the Configuration register (CONFIG).
- Optionally, enable the asynchronous mode.
- Optionally, enable the debouncer mode.
- Enable the EIC by writing a
‘
1’ to CTRLA.ENABLE.
The following bits are enable-protected,
meaning that it can only be written when the EIC is disabled
(CTRLA.ENABLE=0):
- Clock Selection bit in Control A register (CTRLA.CKSEL)
The following registers are enable-protected:
- Event Control register (EVCTRL)
- Configuration register (CONFIG)
- External Interrupt Asynchronous Mode register (ASYNCH)
-
Debouncer Enable register (DEBOUNCEN)
-
Debounce Prescaler register (DPRESCALER)
Enable-protected bits in the CTRLA register
can be written at the same time when setting CTRLA.ENABLE to ‘1’, but not
at the same time as CTRLA.ENABLE is being cleared.
Enable-protection is denoted by the “Enable-Protected” property in the register description.
See NMICTRL, CTRLA, CONFIG, ASYNCH, DEBOUNCEN, DPRESCALER, EVCTRL registers in the EIC Register Summary from Related Links.