13.6 Dream Mode
When the DRMEN bit in the OSCCON register is set, it allows the DMA controller to switch between the Idle mode and the Sleep mode. When the OSCCON.SLPEN bit is set and the OSCCON.DRMEN bit is set, the CRU monitors the DMAC to make sure all transfers are complete before going into the Sleep mode.
If OSCCON.SLPEN = 1, OSCCON.DRMEN = 1, and peripheral clock
requests are active, the CRU goes into the Idle mode until all peripheral clock requests
are non-active; at which time the CRU goes into the Sleep mode.
If OSCCON.SLPEN is not set, the DRMEN bit has no affect as the DMA clocks are still running in the Idle mode.
If the CRU recognizes a wake/interrupt event whose priority will wake the DMA but not the CPU, the CRU transitions to the Idle mode. Therefore, the DMA can perform the needed operations and, when the DMA is finished, the CRU will go back to the Sleep mode. During this time, the CPU is still asleep.
If the wake event is such that the CPU must handle the event, the whole system will exit the Sleep mode and transition back to the Run mode.