4.6.2 External Antenna Placement Recommendations

The following recommendations must be applied for the placement of the antenna and its cable:

  • The antenna cable must not be routed over circuits generating electrical noise on the host board or alongside or underneath the module. It is preferred that the cable is routed straight out of the module.
  • The antenna must not be placed in direct contact or in close proximity of the plastic casing/objects (except when the selected antenna specifically recommends it).
  • Do not enclose the antenna within a metal shield.
  • Keep any components that may radiate noise, signals or harmonics within the 2.4-2.5 GHz frequency band away from the antenna and, if possible, shield those components. Any noise radiated from the host board in this frequency band degrades the sensitivity of the module.
  • The antenna must be placed at a distance greater than 5 cm away from the module. The following figure illustrates the antenna keepout area where the antenna must not be placed.

These recommendations are based on an open-air measurement and do not take into account any metal shielding of the customer end product. When a metal enclosure is used, the antenna can be located closer to the WBZ45 module.

Note: These are generic guidelines, and it is recommended that customers check and fine-tune the antenna positioning in the final host product based on RF performance.
The following figure illustrates an indication on how to route the antenna cable depending on the location of the antenna with respect to the WBZ45 PCB; there are two possible options for the optimum routing of the cable.
Figure 4-22. WBZ45 Antenna Placement Guidelines
Table 4-5. List of Certified Antenna
Serial NumberPart NumberVendorAntenna TypeGainComment
1W3525B039PulsePCB2 dBiCable length 100 mm
2001-0016LSRPIFA2.5 dBiFlex PIFA antenna
3001-0001LSRDipole2 dBiRPSMA connector*
41461530100MolexPCB3 dBi100 mm (Dual Band)
5ANT-2.4-LPW-125Linx TechnologiesDipole2.8 dBi125 mm
6RFA-02-P05-D034AleadPCB2 dBi150 mm
7RFA-02-P33-D034AleadPCB2 dBi150 mm
8ABAR1504-S2450ABRACONPCB2.28 dBi250 mm
9WBZ451 LGA——2.36 dBiOnly for WBZ451 module
10WBZ451H LGAMicrochipPCB4.08 dBiOn-board PCB antenna
11WBZ450 LGA——4.14 dBiOnly for WBZ450 module