38.6.3.4 DMA Interrupt Generation

The DMA Controller operation sets the following interrupt flags in the layer Interrupt Status registers:

  • END—indicates that the current frame DMA transfer is completed.
  • ERROR—indicates that a bus transfer error has been detected.
  • OVF—indicates that a DMA transfer is still pending at the end of frame.