4.10.2.2 Security Network NAS Configuration
The Network Access Server Configuration page allows you to configure the IEEE 802.1X and MAC-based authentication system and port settings, as shown in Figure 4-39. The IEEE 802.1X standard defines a port-based access control procedure that prevents unauthorized access to a network by requiring users to first submit credentials for authentication. One or more central servers, the backend servers, determine whether the user is allowed access to the network. These backend (RADIUS) servers are configured on the Configuration > Security > AAA page. The IEEE 802.1X standard defines port-based operation, but non-standard variants overcome security limitations. MAC-based authentication allows for authentication of more than one user on the same port and does not require the user to have special 802.1X supplicant software installed on his system. The switch uses the user's MAC address to authenticate against the backend server. Intruders can create counterfeit MAC addresses, which makes MAC-based authentication less secure than 802.1X authentication. The NAS configuration consists of two sections, a system-wide and a port-wide.

The Network Access Server Configuration page has the following parameters:
- System Configuration:
- Mode: Indicates if NAS is globally enabled or disabled on the switch. If globally disabled, then all ports are allowed forwarding of frames.
- Reauthentication Enabled: If checked, successfully authenticated supplicants/clients are reauthenticated after the interval specified by the Reauthentication Period. Reauthentication for 802.1X-enabled ports can be used to detect if a new device is plugged into a switch port or if a supplicant is no longer attached. For MAC-based ports, reauthentication is only useful if the RADIUS server configuration has changed. It does not involve communication between the switch and the client, and therefore does not imply that a client is still present in a port. See Aging Period).
- Reauthentication Period: Determines the period in seconds, after which a connected client must be reauthenticated. This is only active if the Reauthentication Enabled checkbox is selected. Valid values are in the range 1s–3600s.
- EAPOL Timeout: Determines the time for retransmission of Request Identity EAPOL frames. Valid values are in the range 1s–65535s. This has no effect for MAC-based ports.
- Aging Period: This setting
applies to the following modes, that is, the modes using the Port Security functionality
to secure MAC addresses:
- Single 802.1X
- Multi 802.1X
- MAC-Based Auth.
When the NAS module uses the Port Security module to secure MAC addresses, the Port Security module must check for activity on the MAC address in question at regular intervals and free resources if no activity is seen within a given period. This parameter controls this period exactly and is set to a number between 10s–1000000s. If reauthentication is enabled and the port is in an 802.1X-based mode, then this is not so critical, as supplicants that are no longer attached to the port get removed upon the next reauthentication, which fails. But, if reauthentication is not enabled, the only way to free resources is by aging the entries. For ports in MAC-based Auth. mode, reauthentication does not cause direct communication between the switch and the client. Therefore, it does not detect if the client is still attached or not, and the only way to free any resources is to age the entry.
- Hold Time: This setting applies to the following modes, that is, modes using the Port Security functionality to secure MAC addresses:
- Single 802.1X
- Multi 802.1X
- MAC-Based Auth.
If a client is denied access—either because the RADIUS server denies the client access or because the RADIUS server request times out (according to the timeout specified on the Configuration > Security > AAA page), the client is put on hold in the Unauthorized state. The hold timer does not count during an on-going authentication. In MAC-based Auth. mode, the switch ignores new frames coming from the client during the hold time. The Hold Time can be set to a number between 10s–1000000s.
RADIUS-Assigned QoS Enabled: RADIUS-assigned QoS provides a means to centrally control the traffic class to which traffic coming from a successfully authenticated supplicant is assigned on the switch. The RADIUS server must be configured to transmit special RADIUS attributes to take advantage of this feature.
The RADIUS-Assigned QoS Enabled checkbox provides a quick way to globally enable/disable RADIUS-server assigned QoS Class functionality. When checked, the individual ports' ditto setting determines whether RADIUS-assigned QoS Class is enabled on that port. When unchecked, RADIUS-server assigned QoS Class is disabled on all ports.
- RADIUS-Assigned VLAN Enabled: RADIUS-assigned VLAN provides a means to centrally control the VLAN on which a successfully authenticated supplicant is placed on the switch. Incoming traffic is classified to and switched on the RADIUS-assigned VLAN. The RADIUS server must be configured to transmit special RADIUS attributes to take advantage of this feature (see RADIUS-Assigned VLAN Enabled for a detailed description). The RADIUS-Assigned VLAN Enabled checkbox provides a quick way to globally enable/disable RADIUS-server assigned VLAN functionality. When checked, the individual port's ditto setting determines whether RADIUS-assigned VLAN is enabled on that port. When unchecked, RADIUS-server assigned VLAN is disabled on all ports.
- Guest VLAN ID: This is the value that a port's Port VLAN ID is set to if a port is moved into the Guest VLAN. It is only changeable if the Guest VLAN option is globally enabled. Valid values are in the range [1; 4095].
- Max. Reauth. Count: The number of times the switch transmits an EAPOL Request Identity frame without response before considering entering the Guest VLAN is adjusted with this setting. The value can only be changed if the Guest VLAN option is globally enabled. Valid values are in the range [1; 255].
- Allow Guest VLAN if EAPOL Seen: The switch remembers if an EAPOL frame has been received on the port for the lifetime of the port. Once the switch considers entering the Guest VLAN, it first checks if this option is enabled or disabled. If disabled (unchecked; default), the switch only enters the Guest VLAN if an EAPOL frame has not been received on the port for the lifetime of the port. If enabled (checked), the switch considers entering the Guest VLAN even if an EAPOL frame has been received on the port for the lifetime of the port. The value can only be changed if the Guest VLAN option is globally enabled.
- Port Configuration: The table has one row for each port on the switch and several columns, which are as follows:
- Port: The port number for which the following configuration applies
- Admin State: If NAS is
globally enabled, this selection controls the port's authentication mode. The following
modes are available:
- Force Authorized: In this mode, the switch sends one EAPOL Success frame when the port link comes up, and any client on the port is allowed network access without authentication.
- Force Unauthorized: In this mode, the switch sends one EAPOL Failure frame when the port link comes up, and any client on the port is disallowed network access.
- Port-based
802.1X: In the 802.1X-world, the user is called the supplicant, the
switch is the authenticator, and the RADIUS server is the authentication server. The
authenticator acts as the man-in-the-middle, forwarding requests and responses
between the supplicant and the authentication server. Frames sent between the
supplicant and the switch are special 802.1X frames, known as EAP Over LANs (EAPOL)
frames. EAPOL frames encapsulate EAP PDUs (RFC3748). Frames sent between the switch
and the RADIUS server are RADIUS packets. RADIUS packets also encapsulate EAP PDUs
together with other attributes like the switch's IP address, name, and the
supplicant's port number on the switch. EAP is very flexible and allows for
different authentication methods, like MD5-Challenge, PEAP, and TLS. The important
thing is that the authenticator (the switch) does not need to know which
authentication method the supplicant and the authentication server are using, or how
many information exchange frames are needed for a particular method. The switch
simply encapsulates the EAP part of the frame into the relevant type (EAPOL or
RADIUS) and forwards it. When authentication is complete, the RADIUS server sends a
special packet containing a success or failure indication. Besides forwarding this
decision to the supplicant, the switch uses it to open or block traffic on the
switch port connected to the supplicant.
For example, if two backend servers are enabled and that the server timeout is configured to X seconds (using the Authentication, Authorization and Accounting (AAA) configuration page) and suppose that the first server in the list is currently down (but not considered dead). Now, if the supplicant retransmits EAPOL Start frames at a rate faster than X seconds, then it never gets authenticated, because the switch cancels on-going backend authentication server requests when it receives a new EAPOL Start frame from the supplicant. As the server has not yet failed (because the X seconds have not expired), the same server is contacted upon the next backend authentication server request from the switch. This scenario loops forever. Therefore, the server timeout must be smaller than the supplicant's EAPOL Start frame retransmission rate.
- Single 802.1X: In port-based 802.1X authentication, once a supplicant is successfully authenticated on a port, the whole port is opened for network traffic. This allows other clients that are connected to the port (for instance through a hub) to piggy-back on the successfully authenticated client and get network access even though they are not authenticated. To overcome this security breach, use the Single 802.1X variant. Single 802.1X is not an IEEE standard but features many of the same characteristics as does port-based 802.1X. In Single 802.1X, at most one supplicant can get authenticated on the port at a time. Normal EAPOL frames are used in the communication between the supplicant and the switch. If more than one supplicant is connected to a port, the one that comes first when the port's link comes up is the first one considered. If that supplicant does not provide valid credentials within a certain amount of time, another supplicant gets a chance. Once a supplicant is successfully authenticated, only that supplicant is allowed access. This is the most secure of all the supported modes. In this mode, the Port Security module is used to secure a supplicant's MAC address once successfully authenticated.
- Multi 802.1X: Multi 802.1X is like Single 802.1X—it is not an IEEE standard, but a variant that features many of the same characteristics. In Multi 802.1X, one or more supplicants can get authenticated on the same port at the same time. Each supplicant is authenticated individually and secured in the MAC table using the Port Security module. In Multi 802.1X, it is not possible to use the multicast BPDU MAC address as destination MAC address for EAPOL frames sent from the switch towards the supplicant, as that causes all supplicants attached to the port to reply to requests sent from the switch. Instead, the switch uses the supplicant's MAC address, which is obtained from the first EAPOL Start or EAPOL Response Identity frame sent by the supplicant. An exception to this is when no supplicants are attached. In this case, the switch sends EAPOL Request Identity frames using the BPDU multicast MAC address as destination: to wake up any supplicants that might be on the port. The maximum number of supplicants that can be attached to a port can be limited using the Port Security Limit Control functionality.
- MAC-based Auth: Unlike port-based 802.1X, MAC-based authentication is not a standard, but merely a best-practices method adopted by the industry. In MAC-based authentication, users are called clients, and the switch acts as the supplicant on behalf of clients. The initial frame (any kind of frame) sent by a client is snooped by the switch, which in turn uses the client's MAC address as both username and password in the subsequent EAP exchange with the RADIUS server. The 6-byte MAC address is converted to a string on the following form xx-xx-xx-xx-xx-xx, that is, a dash (-) is used as separator between the lower-cased hexadecimal digits. The switch only supports the MD5-Challenge authentication method, so the RADIUS server must be configured accordingly. When authentication is complete, the RADIUS server sends a success or failure indication, which in turn causes the switch to open or block traffic for that particular client, using the Port Security module. Only then, the frames from the client can be forwarded on the switch. There are no EAPOL frames involved in this authentication, and therefore, MAC-based Authentication has nothing to do with the 802.1X standard. The advantage of MAC-based authentication over 802.1X-based authentication is that the clients don't need special supplicant software to authenticate. The disadvantage is that MAC addresses can be spoofed by malicious users: Equipment whose MAC address is a valid RADIUS user can be used by anyone. Also, only the MD5-Challenge method is supported. The maximum number of clients that can be attached to a port can be limited using the Port Security Limit Control functionality.
- RADIUS-Assigned QoS
Enabled: When RADIUS-Assigned QoS is both globally enabled and enabled
(checked) on a given port, the switch reacts to QoS Class information carried in the
RADIUS Access-Accept packet transmitted by the RADIUS server when a supplicant is
successfully authenticated. If present and valid, traffic received on the supplicant's
port is classified to the given QoS Class. If (re-)authentication fails or the RADIUS
Access-Accept packet no longer carries a QoS Class or it's invalid, or the supplicant is
otherwise no longer present on the port, the port's QoS Class is immediately reverted to
the original QoS Class (which may be changed by the administrator in the meanwhile
without affecting the RADIUS-assigned).
This option is only available for single-client modes:
-
Port-based 802.1X
Single 802.1X
RADIUS Attributes Used in Identifying a QoS ClassThe User-Priority-Table attribute defined in RFC4675 forms the basis for identifying the QoS Class in an Access-Accept packet. Only the first occurrence of the attribute in the packet is considered, and to be valid, it must follow this rule: All eight octets in the attribute's value must be identical and consist of ASCII characters in the range 0: 7, which translates into the desired QoS Class in the range [0; 7].
-
- RADIUS-Assigned VLAN
Enabled: When RADIUS-Assigned VLAN is both globally enabled and enabled
(checked) for a given port, the switch reacts to VLAN ID information carried in the
RADIUS Access-Accept packet transmitted by the RADIUS server when a supplicant is
successfully authenticated. If present and valid, the port's Port VLAN ID is changed to
this VLAN ID, the port is set to be a member of that VLAN ID, and the port is forced
into VLAN unaware mode. Once assigned, all traffic arriving on the port is classified
and switched on the RADIUS-assigned VLAN ID. If (re-)authentication fails or the RADIUS
Access-Accept packet no longer carries a VLAN ID, it is invalid, or the supplicant is
otherwise no longer present on the port, then the port's VLAN ID is immediately reverted
to the original VLAN ID (which may be changed by the administrator in the meanwhile
without affecting the RADIUS-assigned).
This option is only available for single-client modes:
-
Port-based 802.1X
-
Single 802.1X
For trouble shooting VLAN assignments, use the Monitor > VLANs > VLAN Membership and VLAN Port pages. These pages show which modules have (temporarily) overridden the current Port VLAN configuration.
RADIUS attributes used in identifying a VLAN ID:
RFC2868 and RFC3580 form the basis for the attributes used in identifying a VLAN ID in an Access-Accept packet. The following criteria are used:
- The
Tunnel-Medium-Type,Tunnel-Type, andTunnel-Private-Group-IDattributes must all be present at least once in the Access-Accept packet. - The switch looks for the first
set of these attributes that have the same
Tagvalue and fulfil the following requirements (ifTag== 0 is used, theTunnel-Private-Group-IDdoes not need to include aTag):- Value of
Tunnel-Medium-Typemust be set to IEEE-802 (ordinal 6) - Value of
Tunnel-Typemust be set to VLAN (ordinal 13) - Value of
Tunnel-Private-Group-IDmust be a string of ASCII chars in the range 0: 9, which is interpreted as a decimal string representing the VLAN ID. Leading 0s are discarded. The final value must be in the range [1; 4095].
- Value of
- The
-
- Guest VLAN Enabled: When
Guest VLAN is both globally enabled and enabled (checked) for a given port, then the
switch considers moving the port into the Guest VLAN according to the following rules.
This option is only available for EAPOL-based modes:
-
Port-based 802.1X
-
Single 802.1X
-
Multi 802.1X
For trouble shooting VLAN assignments, use the Monitor > VLANs > VLAN Membership and VLAN Port pages. These pages show which modules have (temporarily) overridden the current Port VLAN configuration.
Guest VLAN Operation
When a Guest VLAN enabled port's link comes up, the switch starts transmitting EAPOL Request Identity frames. If the number of transmissions of such frames exceeds Max. Reauth. count and no EAPOL frames have been received, the switch considers entering the Guest VLAN. The interval between transmission of EAPOL Request Identity frames is configured with EAPOL Timeout. If Allow Guest VLAN if EAPOL Seen is enabled, then the port is placed in the Guest VLAN. If disabled, the switch first checks its history to see if an EAPOL frame has previously been received on the port (this history is cleared if the port link goes down or the port's Admin State is changed), and if not, the port is placed in the Guest VLAN. Otherwise, it does not move to the Guest VLAN but continues to transmit EAPOL Request Identity frames at the rate given by EAPOL Timeout. Once in the Guest VLAN, the port is considered authenticated, and all attached clients on the port are allowed access on this VLAN. The switch does not transmit an EAPOL Success frame when entering the Guest VLAN. While in the Guest VLAN, the switch monitors the link for EAPOL frames, and if one such frame is received, then the switch immediately takes the port out of the Guest VLAN and starts authenticating the supplicant according to the port mode. If an EAPOL frame is received, then the port is never able to go back into the Guest VLAN, if Allow Guest VLAN if EAPOL Seen is disabled.
-
- Port State: The current
state of the port. It can undertake one of the following values:
- Globally Disabled: NAS is globally disabled
- Link Down: NAS is globally enabled, but there is no link on the port
- Authorized: The port is in Force Authorized or a single-supplicant mode and the supplicant is authorized
- Unauthorized: The port is in Force Unauthorized or a single-supplicant mode and the supplicant is not successfully authorized by the RADIUS server
- X Auth/Y Unauth: The port is in a multi-supplicant mode. Currently, X clients are authorized and Y are unauthorized.
- Restart: Two buttons are
available for each row. The buttons are only enabled when authentication is globally
enabled, and the port's Admin State is in an EAPOL-based or MAC-based mode. Clicking
these buttons does not cause settings change on the page to take effect.
- Reauthenticate: Schedules a reauthentication when the quiet-period of the port runs out (EAPOL-based authentication). For MAC-based authentication, reauthentication is attempted immediately. The button only has the effect for successfully authenticated clients on the port and does not cause the clients to get temporarily unauthorized.
- Reinitialize: Forces a reinitialization of the clients on the port and thereby a reauthentication immediately. The clients transfer to the unauthorized state while the reauthentication is in progress.