BLE_GAP_ExtAdvParams_T
C
typedef struct BLE_GAP_ExtAdvParams_T { uint8_t advHandle; uint16_t evtProperies; uint32_t priIntervalMin; uint32_t priIntervalMax; uint8_t priChannelMap; BLE_GAP_Addr_T peerAddr; uint8_t filterPolicy; int8_t txPower; uint8_t priPhy; uint8_t secMaxSkip; uint8_t secPhy; uint8_t sid; bool scanReqNotifiEnable; } BLE_GAP_ExtAdvParams_T;
Description
Structure for configuring extended advertising parameters.
Field Documentation
Field | Description |
---|---|
advHandle | Identifies the advertising set whose parameters are being configured. Valid range: 0 to 0xEF. Refer to Maximum advertising handle for the maximum value. |
evtProperies | The type of advertising event that is being configured and its properties. Combinations of bits from Extended advertising event properties are used to define the event properties. |
priIntervalMin | Minimum primary advertising interval. Valid range: 0x20 to 0x1F4000. Unit: 0.625 ms. Refer to Extended primary advertising interval range for more details. |
priIntervalMax | Maximum primary advertising interval. Valid range: 0x20 to 0x1F4000. Unit: 0.625 ms. Refer to Extended primary advertising interval range for more details. |
priChannelMap | Bitfield indicating the advertising channels to be used. Refer to Advertising channels for channel definitions. Note: Advertising channels_ALL is not permitted. |
peerAddr | Remote Bluetooth address and address type. Refer to BLE_GAP_Addr_T for structure details. |
filterPolicy | Advertising filter policy. Refer to Advertising filter policies for possible values. |
txPower | The maximum transmit power level for advertising packets on the advertising channels. Set to 0x7F if no preference is specified. The level will be adjusted if the value is out of range. |
priPhy | The PHY on which the advertising packets are transmitted on the primary advertising channel. Note: 2M PHY cannot be used for primary advertising. Refer to PHY types for possible values. |
secMaxSkip | The maximum number of advertising events that can be skipped before sending an AUX_ADV_IND. |
secPhy | The PHY on which the advertising packets are transmitted on the secondary advertising channel. Refer to PHY types for possible values. |
sid | The value to be transmitted in the Advertising SID subfield of the ADI field in the Extended Header. Refer to Advertising Set Identifier (SID) range for the valid range. |
scanReqNotifiEnable | Indicates whether notifications should be sent upon receipt of a scan request PDU. Set to true to enable notifications, or false to disable them. |