6.6 MPMF 1x4 Fixture Board Design
Perform the following configuration in the MPMF configuration window.
- Browse and load the MPMF
*.msffile (see following figure). - From the “Write Mode” drop-down list, choose IBDK Mode.
- Select the interface and choose the COM port from the "COM" drop-down list (see following figure).
- Check the Log Directory check box.
- Click Apply to finish the
configuration.
Figure 6-11. MPMF Configuration - In the MPMF main page, click RUN to run the Flash download on the device.
The MPMF test tool supports up to two 1x4 test fixture, that is, the user can execute the eight DUT Flash downloads simultaneously.