45.5.18 Energy Efficient Ethernet Support
Features
- Energy Efficient Ethernet according to IEEE 802.3az
- A system’s transmit path can enter a low power mode if there is nothing to transmit.
- A PHY can detect whether its link partner’s transmit path is in low power mode, and configure its own receive path to enter low power mode.
- Link remains up during lower power mode and no frames are dropped.
- Asymmetric, one direction can be in low power mode while the other is transmitting normally.
- LPI (Low Power Idle) signaling is
used to control entry and exit to and from low power modes. Note: LPI signaling can only take place if both sides have indicated support for it through auto-negotiation.
Operation
- Low power control is done at the RMII (reconciliation sublayer).
- As an architectural convenience in writing the 802.3az it is assumed that transmission is deferred by asserting carrier sense - in practice it will not be done this way. This system will know when it has nothing to transmit and only enter low power mode when it is not transmitting.
- LPI should not be requested unless the link has been up for at least one second.
- LPI is signaled on the RMII transmit path by asserting 0x01 on TXD with TX_EN low and TX_ER high.
- A PHY on seeing LPI requested on the RMII will send the sleep signal before going quiet. After going quiet it will periodically emit refresh signals.
- The sleep, quiet and refresh periods are defined in 802.3az, Table 78-2.
- LPI mode ends by transmitting normal idle for the wake time. There is a default time for this but it can be adjusted in software using the Link Layer Discovery Protocol (LLDP) described in 802.3az, Clause 79.
- LPI is indicated at the receive side when sleep and refresh signaling has been detected.