Defines the analog offset to be used for channel CSEL (configured in the AFEC Channel Selection Register). This value is used as an input value for the DAC included in the AFE.
Note: The field AOFF must be configured
to 512 (mid scale of the DAC) when there is no offset error to compensate. To
compensate for an offset error of n LSB (positive or negative), the field AOFF must
be configured to 512 + n.
The value of the AOFF bit can be updated only if the AFEC
module is restarted, or if two conversions are run; the second one will have the
correct AOFF bit setting.