39.8.3 Read Operation
The following flowchart shows how to read a single block with or without use of DMAC facilities. In this example, a polling method is used to wait for the end of read. Similarly, the user can configure the HSMCI Interrupt Enable Register (HSMCI_IER) to trigger an interrupt at the end of read.
Note:
- It is assumed that this command has been correctly sent (see the Command/Response Functional Flow Diagram).