17.7 Clearing Interrupt Flags
The individual status flags, (IOCAFx, IOCBFx, IOCCFx and IOCEF3) bits, can be cleared by resetting them to zero. If another edge is detected during this clearing operation, the associated status flag will be set at the end of the sequence, regardless of the value actually being written.
In order to ensure that no detected edge is lost while clearing
flags, only AND operations masking out known changed bits should be
performed. The following sequence is an example of what should be performed.
Clearing Interrupt Flags (PORTA Example)
MOVLW 0xff
XORWF IOCAF, W
ANDWF IOCAF, F