addCommand
addCommand(barSeparatedCmdPath ,
funcToCall)
Insert a menu entry in the project view. The menu hierarchy is described by bar
| separated submenus. The last string is shown as the command to
invoke. When double clicked by the user, MPLAB X IDE will execute
the function funcToCall.
Example
def onload(ide):
ide.addCommand("Test|msg|Print example", "print_hello")
ide.addCommand("Device actions|Set DAL 0", "set_dal_0")
ide.addCommand("Device actions|Chip Erase", "chip_erase_l10")
def set_dal_0():
if deb.Connected():
r = msg.msg("Debugger is in use. Stop debugging and retry", "Busy")
return
deb.Connect()
try:
dev.Write32... # send commands to NVM controller to set DAL 0
finally:
deb.Disconnect()
Commands for the build process follow.