6.5.1.1 Manage Configurations Dialog
To create your own configuration, start by doing one of the following:
- Use the drop down menu on the toolbar and select
Customize. The Project Properties
window will open.

- Open the Project Properties window by right clicking on the project name and selecting Properties.
In the Project Properties window, click Manage Configurations to open the Configurations dialog. Existing configurations can be renamed or a new configuration can be added or duplicated from an existing one. Any spaces in the name will be replaced with underscores.
When more than one configuration is created for a project, the active one can be selected from Manage Configurations or from the drop-down menu.