6.5.1.7 Configuration Macros
When you add a new or duplicate configuration, you can create your own
configuration-related macros or use autogenerated macros for #ifdef or
other statements in code. These are MPLAB XC C compiler preprocessor macros.
User-Defined Macros
To define your own preprocessor macro:
- In the Project Properties window, click on a project configuration to make it active. Under that configuration, click on the compiler in the toolchain.
- Under the Preprocessing and messages options category, locate the option that allows you to define a macro and click on the associated text box.
- In the pop-up dialog, enter a macro name and click
OK. This macro is now associated with the active
configuration.
You can name the macro the same as a configuration (such as My_Debug from Add a Duplicate Configuration) or you can give it any other name (such as DebugConfig).
Macro names (and strings, discussed below) are case-sensitive.
You can now use the preprocessor macro in conditional text:
// If My_Debug configuration is active
#ifdef DebugConfig
fprintf(stderr,"This is a debugging message\n");
#endif
In addition, you can assign a string value that matches the configuration name to your macro(s) for use in regular code:
#ifdef DebugConfig
#define CFG_NAME “My_Debug”;
// other defines
#endif
#ifdef DefaultConfig
#define CFG_NAME “My_Default”;
// other defines
#endif
:
int main(int argc, char** argv)
{
printf(CFG_NAME);
return{EXIT_SUCCESS};
}
The CFG_NAME macro will always hold the active
configuration's name.
Autogenerated Macros
When a new or duplicate configuration is created, for example
My_Test, a related macro is also created, for example
XPRJ_My_Test. The macro will have a string value which matches the
name of the configuration (My_Test).
You can use the macro for #ifdef statements as in the
previous section, or you can use the value of the macros at compile time as follows:
int main(int argc, char** argv)
{
printf(CFG_NAME);
return{EXIT_SUCCESS};
}
The CFG_NAME macro will automatically hold the active
configuration's name.