3.4.9.3.1 Set Up the Warrant File
Before starting the key export, make sure to copy the HSM module warrant file from nCipher into the Tools directory. This file contains a cryptogram that identifies the origin of the HSM module. The file name follows the format:
warrant-[ESN].txt
Here, ESN is the module serial number that can be printed using the nfkminfo
utility. The following is an example of the warrant file copied
into the Tools directory:
C:\Microsemi\Tools\warrant-586F-B963-9146.txt