12 Appendix 2: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory TCL_Scripts. If required, the design flow can be reproduced from Design Implementation till generation of job file.
Following are the steps to run the TCL:
- Launch the Libero software
- Select
- Click Browse
and select
script.tclfrom the downloaded TCL_Scripts directory. - Click Run.
After successful execution of TCL script, Libero project is created within TCL_Scripts directory.
For more information about TCL scripts, see mpf_an4949_v2022p3_df/TCL_Scripts/readme.txt.
For more details on TCL commands, see Tcl Commands Reference Guide . Contact Technical Support for any queries encountered when running the TCL script.