11 Appendix 1: Programming the Device Using FlashPro Express
(Ask a Question)This chapter describes how to program the PolarFire device with the Job
programming file using a FlashPro programmer. The default location of the
.stp file is
mpf_an4949_v2022p3_df\Programming_Job.
To program the PolarFire device using FlashPro Express, perform the
following steps:
- Ensure that the jumper settings on
the board are the same as listed in Table 9-3.Tip: The power supply switch must be switched OFF while making the jumper connections.
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to the J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- On the host PC, launch the FlashPro Express software.
- Click New or
select New Job Project from FlashPro Express
Job from Project menu to create a new job
project. See the following figure.
Figure 11-1. FlashPro Express Job Project - Enter the following in the
New Job Project from FlashPro Express Job dialog box:
- Programming job file: Click Browse, and navigate to the location where the .job file is located and select the file. The default location is <download_folder>\mpf_an4949_v2022p3_df\Programming_Job.
- FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
Figure 11-2. New Job Project from FlashPro Express Job
- Click OK. The required programming file is selected and ready to be programmed in the device.
- The FlashPro Express window appears.
Confirm that a programmer number appears in the Programmer field. If it does not,
confirm the board connections and click Refresh/Rescan
Programmers.
Figure 11-3. Programming the Device - Click RUN.
When the device is programmed successfully, a RUN PASSED
status is displayed.
Figure 11-4. FlashPro Express—RUN PASSED - Close FlashPro Express or in the Project tab, click Exit.