9 Libero Design Flow
(Ask a Question)This section describes the Libero design flow, which involves the following processes:
- Synthesis
- Place and Route
- Verify Timing
- Design and Memory Initialization
- Generate Bitstream
- Run Program ActionImportant: To initialize TCM in PolarFire using system controller, a local parameter, l_cfg_hard_tcm0_en, in the miv_rv32_opsrv_cfg_pkg.v file must be changed to 1’b1 prior to synthesis. See, MIV_RV32.
The following figure shows these options in the Design Flow window.