10.4.2.2.3 Changing the Clock Frequency and Duty Cycle

The selected clock source for a Generator can be divided by writing to the Division Factor bit field of the Generator Control register (GENCTRL[n].DIV). The actual division factor is determined by the divide selection bit of the GENCTRL[n] register (GENCTRL[n].DIVSEL).

When dividing a clock with an odd division factor, the duty-cycle will not be 50/50. Writing ‘1’ to the improve duty cycle bit of the GENCTRL[n] register (GENCTRL[n].IDC) will result in a 50/50 duty cycle.

The resulting clock frequency fGCLK is calculated as follows:
  • If GENCTRL[n].DIVSEL = ' 0’ and GENCTRL[n].DIV is either ‘0x0’ or ‘0x1’, the output clock will not be divided
  • If GENCTRL[n].DIVSEL is ‘0’ then the resulting frequency of the GCLK is calculated as follows:

    fGCLK⁢= GENCTRLn.SRCDIV

    • If GENCTRL[n].DIV is an odd number, the Improve Duty Cycle bit of the GENCTRL[n] register (GENCTRL[n].IDC) must be set to ‘1’
    • If GENCTRL[n].DIV is an even number, the GENCTRL[n].IDC bit must be ‘0’
  • If GENCTRL[n].DIVSEL is ‘1’ then the resulting frequency of the GCLK is calculated as follows:

    fGCLK⁢= GENCTRLn.SRC2(DIV⁢+ 1)

    • GENCTRL[n].IDC must always be ‘0’

The following table shows the number of divider bits associated with each Generator:

Table 10-2. Generator Selection Overview
ValueDescriptionEnabled at Reset?Divider bits (GENCTRLn.DIV)
0x0Generator 0Yes8
0x1Generator 1No16
0x2Generator 2No8
0x3Generator 3No8
0x4 - 0xfReserved--
Note: The size of the DIV bit field may vary from Generator to Generator.