26.5.1 Interrupt Configuration
The Timer module has a dedicated Interrupt Flag bit (TxIF) and a corresponding Interrupt Enable Mask bit (TxIE).
The TxIF bit is set when the timer count matches the respective period register and the timer module is not operational in Gated Time Accumulation mode. This bit is also set if the falling edge of the gate signal is detected when the timer is operating in Gated Time Accumulation mode. The TxIF bit is set, regardless of the state of the corresponding TxIE bit. If required, the TxIF bit can be polled by software.
The TxIE bit is used to define the behavior of the interrupt controller when the TxIF bit is set. When the TxIE bit is clear, the interrupt controller does not generate a CPU interrupt for the event. If the TxIE bit is set, the interrupt controller generates an interrupt to the CPU when the T1IF bit is set (subject to the interrupt priority).
It is the responsibility of the user’s software routine that services a particular interrupt to clear the appropriate interrupt flag bit before the service routine is complete.
The priority of the Timer module can be set with the TxIP[2:0] bits. This priority defines the priority group to which the interrupt source will be assigned. The priority groups range from a value of seven (the highest priority) to a value of zero (which does not generate an interrupt). An interrupt being serviced will be preempted by an interrupt in a higher priority group.
After an enabled interrupt is generated, the CPU will jump to the vector assigned to that interrupt. The vector number for the interrupt is the same as the natural order number. The CPU will then begin executing code at the vector address. The user’s code at this vector address should perform any application-specific operations and clear the TxIF interrupt flag and then exit.