35.3.2 DMT Count Selection
The Deadman Timer count is set by the PSCNT register bits. The current DMT count value can be obtained by reading the DMTCNT register.
The PSCNT[31:0] bits allow the software to read the maximum count selected for the Deadman Timer. Whenever the DMT event occurs, the user can always compare to see whether the current counter value in the DMTCNT register is equal to the value of the PSCNT register, which holds the maximum count value.
The PSINTV[31:0] bits allow the software to read the DMT window interval value. So whenever the DMT current counter value in DMTCNT reaches the value of PSINTV, the window interval opens so that the user can insert the clear sequence to the STEP2 bits, which causes the DMT to reset.
The initial DMT state has the timer cleared; the DMTPRECLR and BAD1/BAD2 flags are cleared. When reset, the DMT clears the DMTSTAT register. When activated, the DMT begins to count whenever an instruction is fetched while clocks are running.