11.3.2 Interrupt Vector Table Collapse
The IVT can be collapsed by configuring the IVTC bit within the IVTCREG register. While
trap handlers remain unaffected by this setting, all peripheral interrupts are directed
to a single location that follows trap vectors. When the IVTC bit is set to
1, all peripheral interrupts utilize a common vector, which is
located at the offset address 0x24.
The collapsed peripheral interrupt vector is placed in the reserved interrupt location. The trap interrupts are not collapsed, and the peripheral interrupts are pointed to one location, which is placed after the trap's interrupt location, as shown in Figure 11-2.
The potential application of remappable and/or collapsible Interrupt Vector Tables is in
scenarios where the processor is operating within a secure or boot memory segment and
encounters a trap or an interrupt. In such cases, the secure boot software is required
to assign the interrupt base address to a designated interrupt vector address located
within the secure or boot memory segment. Upon completion of its operations, the secure
boot software will then assign predetermined values to specific memory segments.
Additionally, the secure boot software has the option to set the Interrupt Vector Table
Collapse (IVTC) to "1", thereby consolidating the interrupt vector for
all peripherals into a single entry. Once the secure boot software has finalized its
processes, it may reset this bit, effectively deactivating the collapsed IVT feature.