8.4.10.2 IRT Firmware

Once IRT is configured as described in Enabling IRT, IRT firmware execution starts immediately after device startup. IRT firmware execution ends when the IRT firmware sets the DONE (IRTCTRL[2]) bit and there is a subsequent instruction fetch from program memory that is NOT within an IRT region. Note that this includes an attempted instruction fetch that has an error, such as an access privilege violation or an uncorrectable bit error.

The IRT firmware may set the DONE bit and transfer control to the application code (non-secure) while executing from an IRT region. Once the IRT code sets the DONE bit and vectors to non-IRT space, PLCK will be set, and the regions will become inaccessible.

Note: The IRT firmware must ensure that the application code is not prefetched before the DONE bit is set. This requirement can be met by having at least 32 bytes of separation between the end of the IRT firmware and the start of the application firmware. This ensures that the start of the application code is fetched after the DONE bit is set, disabling the IRT partition before the application code can execute. The IRT firmware must ensure that the application start address is in user program Flash and not within an IRT region.
Note: It is recommended to develop the IRT firmware separately from the non-IRT firmware. To do this, create separate MPLAB projects for the IRT and non-IRT firmware. The IRT project can then be added as a loadable in the non-IRT project. The non-IRT project may also use a custom linker script to exclude the IRT region as available Flash memory to avoid overlapping with IRT code.