3.6.8.8.1 NaN Propagation Operand Detection

For instructions that generate a result, special propagation rules apply when one or both source operands are NaN values, such that sNaNs can be successfully used as “tracer” values. If a NaN is deemed to be propagated, then it will replace the operation result.

With reference to NaN Propagation , all instructions will examine the operands for NaN values during the RD-stage.

  • Two operand instructions:

    If one or both operands are NaN values, the RD-stage will apply a propagation priority as shown in Table 3-13 .

  • Three operand FMAC instructions:

    The source operands are examined in the RD-stage as usual, but in conjunction with the selected intermediate result, and any NaN values detected are propagated as shown in Table 3-14 .

  • Three operand FFLIM instructions:

    If one or both limit operands are NaN values, the RD-stage will apply a propagation priority as shown in Table 3-12 . If the FFLIM input value is a NaN, the limit values are ignored, and the input NaN value is propagated (quieted if an sNaN).

    In all cases, if a NaN is to be propagated, the corresponding NaN value is entered as the operand value in the Instruction/Hazard Tracker FIFO entry for that instruction. The instruction FIFO entry also sets a flag to indicate that NaN propagation is enabled.