External RAW Hazards
An external RAW (Read-After-Write) data dependency hazard will occur should the contents of an FPU register be unavailable at the time it is read by the CPU because the register is bound to a previously issued FPU instruction. The coprocessor will detect the hazard and read will be stalled until such time that the register becomes available (i.e., after the result has be written), creating a read stall for the CPU.
In addition, an external RAW hazard will occur if:
- A CPU write to a coprocessor
register is immediately followed by the CPU issuing a coprocessor instruction
that uses the same register as an operand source.
or
- A CPU write to a coprocessor register is immediately followed by a CPU read of the same register.
In both of these CPU RAW hazard scenarios, the CPU is responsible for detecting the hazard and inserting the necessary stall cycle for the coprocessor to resolve the hazard. Hazard detection is the same for both scenarios.
In order to resolve these hazards, the coprocessor includes data forwarding paths between the CPU W-stage and both the coprocessor RD-stage (as shown in Figure 3-31) and the CPU read data output (as shown in Figure 3-32). These paths will forward the write data value should the write and read instructions target a common register.
CPU write data forwarding to the coprocessor RD-stage allows the CPU to issue a coprocessor instruction earlier than would be possible if the CPU coprocessor write had to complete. CPU write data forwarding to the CPU read data path together with a CPU stall cycle (detected and inserted by the CPU) resolves the (unlikely) hazard that arises when a CPU write is followed immediately by a CPU read of the same coprocessor register. The converse scenario where a CPU read of an FPU register into a W-reg is immediately followed by a CPU write of the same W-reg to another F-reg is shown in Figure 3-33.