4.7.3.4 To Export all Breakpoints that Match the Current Search Criteria
In the Breakpoints window toolbar, click the Export all breakpoints matching the current search criteria icon.
- The Save As dialog box appears.
- In the Save As dialog box, type a name in the File name box.
- This is the name of the XML file that will contain the exported breakpoints. Note the folder path shown at the top of the dialog box. To save the XML file to a different location, change the folder path shown in that box or click Browse Folders to browse for a new location.
- Click Save.