4.8.2.3 Data Breakpoint Configuration Window for XMEGA®

This window provides configuration options related to the data breakpoint for XMEGA devices.
Location
Enter a specific address in RAM (e.g., 0x8004) directly or an expression that evaluates to an address in RAM (e.g., &x). Make sure the expression you enter represents the address of the data to monitor.
Access Mode
Configure the breakpoint to break on the specific Access Mode. Three types of access modes are supported:
- Read - Program breaks on read at a specified location.
- Write (Default) - Program breaks on write at a specified location.
- Read/Write - Program breaks on read or write at a specified location.
Data Match
Use the Data Match option to configure Data Breakpoint to compare the data at a specified location based on one of the following conditions:
- Location content is equal to the value
- Location content is greater than the value
- Location content is less than or equal to the value
- Location content is within the range
- Location content is outside the range
- Bits of the location is equal to the valueNote: Bit Mask: This is an 8-bit value where bits with
'1'are significant, and the bits with'0'are don't care.In general, for a given value V and bitmask M, the break event is triggered when the value in the location field VL satisfies the following condition:
(V) & (M) == (VL) & (M)
For example, using
Value = 0xA0andBit Mask = 0xF0will trigger a break event when the location field has the values between0xA0to0xAF.