4.5.2 Keyboard Shortcut

By default, there is no keyboard shortcut to this function. If frequently used, you might want to add one. To add one, click the Tools → Options menu button and go to Environment → Keyboard. Start typing startwithouttdebugging in the Show commands containing the input field, and select Debug.StartWithoutDebugging in the list. Then select the Press shortcut keys input field, and press the desired key combination. You can, for example, press Ctrl+F5. Note that this shortcut is already assigned to the BreakAll command. If you choose to override it, press the Assign button to assign the new keyboard shortcut. Or, you can select an unused key combination.
Figure 4-4. Add Keyboard Shortcut