10.3.1.1 General Environment Settings
Items Shown in Window Menu
Customizes the number of windows that appear in the Windows list of the Window menu. Type a number between 1 and 24. By default, the number is 10.
Items Shown in Recently Used Lists
Customizes the number of most recently used projects and files that appear on the File menu. Type a number between 1 and 24. By default, the number is 10. This is an easy way to retrieve recently used projects and files.
Automatically Adjust Visual Experience Based on Client Performance
This setting specifies whether Microchip Studio sets the adjustment to the visual experience automatically or if you explicitly set the adjustment. This adjustment may change the display of colors from gradients to flat colors, or it may restrict using animations in menus or pop-up windows.
Enable Rich Client Experience
Enables the complete visual experience of Microchip Studio, including gradients and animations. Clear this option when using Remote Desktop connections or older graphics adapters because these features may have poor performance in those cases. This option is available only when you clear the Automatically adjust visual experience based on the client option.
Use Hardware Graphics Acceleration if Available
Uses hardware graphics acceleration if it is available, rather than software acceleration.
Show Status Bar
Displays the status bar. The status bar is located at the bottom of the IDE window and displays information about the progress of ongoing operations.
Close Button Affects Active Tool Window Only
Specifies that when clicking the Close button, only the tool window that has focus is closed, and not all of the tool windows in the docked set. By default, this option is selected.
Auto Hide Button Affects Active Tool Window Only
Specifies that when clicking the Auto Hide button, only the tool window that has focus is automatically hidden, and not all of the tool windows in the docked set. By default, this option is not selected.
Restore File Associations
Registers file types that are typically associated with Microchip Studio. Registration causes Windows to display the correct icons in Windows Explorer and recognize Microchip Studio as the correct application for opening these file types.
This option can be helpful if you have two different versions of Microchip Studio installed on the same computer, and you later uninstall one of the versions. After uninstalling, the icons for Atmel Studio files no longer appear in Windows Explorer. Also, Windows no longer recognizes Microchip Studio as the default application for editing these files. This option restores those associations.