5.4.1 Power Debugger
The Power Debugger has a single voltage source and two channels of voltage/current measurement.

The voltage output (VOUT) is adjusted by the slider or by typing a voltage in the Generated text boxes below the slider.
After adjusting the set-point, press the Write button to apply the changes. Then the value is sent to the tool, and the measured value is read back.
Press the Read button to read both the set-point (Generated) and the Measured values from the Power Debugger.
The output voltage range is 1.6V to 5.5V.
The Channel A and Channel B measurements are snapshots of analog readings taken by the Power Debugger. The tool is optimized for real-time monitoring of voltage and current, and this snapshot is thus approximate. It does not perform calibration compensation, and readings are locked in the highest-current range. For best results, use the Atmel Data Visualizer.